Feedback_Iq_Min_Threshold
| Index.Sub | 2230.21H |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable |
No |
| Unit |
0.01 rpm |
|
Range |
Unsigned32 |
| Default Value |
18 |
| Store Supported | Yes |
| Description |
This value is used for Closed Loop feature and defines limit speed value under which the Feedback_Iq_min object is enabled to work. |
|
Notes |
This object is not available in EtherCAT fieldbus. |